User Activity

Hi,I am using LIS2DW12 Accelerometer for tilt angle detectionIs it possible to detect the tilt angle(A and B) in both directions as shown in figure and trigger the interrupt event in wakeup interrupt mode?It is possible in 6d orientation mode, but I ...
Hi,I am using LIS2DW12 accelerometer for tilt angle detection.I expect an interrupt event when the tilt angle is crossing the threshold and is working fine.But an interrupt event is unnecessarily occurring during physical shocks/knocks which is not e...
Hi,I am using an accelerometer (LIS2DW12) from STMicroelectronics. An interrupt is generated only for (50,60,70,80) degrees only while setting on 6D orientation mode. I would expect to get an interrupt for even small degrees of tilt starting from 10 ...