User Activity

I have recently downloaded STM32CubeExpansion_LRWAN_V1.2.1.In the main.c of the End_Node example I commented all the sensor related variables etc. and just tried to send letter 'H' with AppData.Buff[i++] = 'H';The message gets though but it keeps cha...
Hey,APP_TX_DUTYCYCLE doesn't really do its job. I set it to 1s and my messages are being sent so that it always skips one. Example:1st message sent, 3rd message sent, 5th mesage sent..Upon increasing the DC parameter it works fine. What is causing th...
Hey!I would like to have a constant spreading factor and bandwidth when my node is transmitting data and I cannot find where I can set these parameters.I thought I would set datarate in RegionEU868.h and control these parameters this way but it doesn...