Too late for you, but I hope to help folks who want to stop SPI Circular precisely. There's no clean way with ST HAL library. You have to do some hacky things. It maybe a good idea not to use the ST SPI code, and just roll your own. Here are the broa...
@Jocelyn RICARD The merge by STM32_Programmer_CLI.exe goes without errors. That's not the issue. The issue is the resulting elf file is bad. The address of the header is wrong. You can use an elf tool to view the resulting elf file and check the ad...
You probably have moved on, but I'll write anyway for people who need it.I faced the same problem with the example from "NUCLEO-H753ZI\Applications\2_Images\2_Images_UserApp".@Jocelyn RICARD The merging of header is done by STM32_Programmer_CLI.exe,...