User Activity

I'm trying to use the internal reference voltage of 2.048V in my application, since I'm powering the microcontroller with 2.8V. But when I select the reference source and enable the VRefBuff with this lines: HAL_SYSCFG_VREFBUF_VoltageScalingConfig(S...
In the datasheet for the TSV711 is sated (p20): 4.8 Macromodel Accurate macromodels of the TSV71x devices are available on the STMicroelectronics’ website at www.st.com.So, where are they??? I looked everywhere, Digikey has a deadlink to the macromod...
I have an application who requires a stable clock source in the whole temperature range but the power budget is tight, so we chose to use the MSI in sync with an external low power 32khz clock.To save extra power we send the core to sleep while it's ...
In the datasheet of the L7987L there is an application schematic for a negative converter (p36), here the VCC is connected to VIN with a 10 Ohm resistor and a capacitor to the generated negative rail (I guess is to filter the power for the low power ...
hi!I found the model for the L7987 (and L too) but it is encrypted for PSpice, but I would like to use this (or any other model for this chip) in LTSpice, exist any unencrypted model for this chip? if not, is there any way to have it unencrypted?