Hello @fpoussin ,One more question, I'm surprised you need to patch the scmi node because, in order to ease the usage of SP-MIN for some customer that want to stay (for now) on SP-MIN, we directly patch the scmi node from SP-MIN (the u-boot DT node)...
Hi @DDing.1 ,Go to know, in the FIP management there is no formal "Authentication success" to be printed.If it boots, it works ;)The only way can you can ensure that it works is that the complete firmware + certificate are loaded:Image 31 (FW_CONFIG...
Hi @DDing.1 Sorry, late reply, try to figure out what append.First thing.The bl2 produce in the fip target is a kind of 'fake' BL2, just used to generate the certificate Trusted_key certificate file used to authenticate FW config and HW config file....
Hi @[DDing.1] ,The wiki as a lack of info, I'll add it soon for the MBEDTLS part.MBEDTLS is used as an external repo as mentioned here in the official doc:https://trustedfirmware-a.readthedocs.io/en/v2.4/design/trusted-board-boot-build.htmlTo build ...
Hi,Your build command looks go to me, but I'm surprised that the build date print into your boot is NOTICE: BL2: Built : 16:43:51, Nov 17 2020.Are you sure to updated it into your card? First partition must be updated with you binary generated, stm32...