User Activity

I am trying to develop an application in C/C++ (QT) to perform an ISO 15693 R2H FTM data transfer with an STDV04 tag using the STR25R3111DISCOComm DLL. I am able to link to the DLL, connect to the DISCO board and perform a passive read on my tag usin...
Hi,I am having a problem using Read Out Protection on the STM32F405VE processorMy firmware has a proprietary bootloader which is stored at 0x8000000. It basically checks to see if a USB OTG lead is plugged in and if so attempts to access a mass stora...
Posted on November 10, 2017 at 16:28I have recently added USB support to a product, using the STM32_USB_Host_Library MSC class taken from the STM32Cube_FW_F2_V1.7.0 examples.We successfully detect devices and write and read from the disk until we ge...
Posted on February 25, 2016 at 19:03Hi, I have hit a rather strange problem that has completely stumped me!I have a really simple bootloader for the STM32L100 device which uses the USB DFU interface to copy new firmware into the flash. The bootloade...
Kudos from