User Activity

Posted on December 09, 2015 at 19:16Hi I am writing some data to an external device on the address and data bus I have used Stm32cube to set up the timing data. Once I have written the data to the device I have to strobe a data line. This is fine bu...
Posted on December 09, 2015 at 19:15Hi I am writing some data to an external device on the address and data bus I have used Stm32cube to set up the timing data. Once I have written the data to the device I have to strobe a data line. This is fine bu...
Posted on December 07, 2015 at 17:13Hi have a SRAM Disk working using FATFS and USB. I can read and write files to the disk from my processor (STM32f427zit)  but the files do not get updated in windows explorer on the PC. If if unplug the USB and th...
Posted on October 30, 2015 at 14:56Hi I am struggling to get the External Audio Clock Input (PC9 12.288MHZ) to be output by the SAI Master clock pin PF7. I have used STM32Cube  to set it up and it all looks ok,  but I can not get any output on the S...
Posted on October 30, 2015 at 14:55Hi I am struggling to get the External Audio Clock Input (PC9 12.288MHZ) to be output by the SAI Master clock pin PF7. I have used STM32Cube  to set it up and it all looks ok,  but I can not get any output on the S...