User Activity

Posted on May 30, 2017 at 01:36The latest version of CubeMX (4.21) with F4 Libs (v1.16) using the SDIO controller seems to have broken FatFS support.  ff.c needs a file that declares the character sets being used because it contains a couple of util...
Posted on December 07, 2016 at 21:47 There is a problem with IDE debuggers for STM32F7, and as I understand, all ARM M7 core based processors. With other CORTEX controllers, when a debbuger pauses or hits a breakpoint, the debugger stops interrupt p...
Posted on May 10, 2016 at 21:08The examples in the CubeMX repository do not use CubeMX to generate init code.  This means that they may be a little useful for showing examples of on-chip and on-board peripherals working, but give little assistance i...
Posted on May 08, 2016 at 11:07It is far from intuitive how to re-create the functionality of the CubeMX example or Application example programs using CubeMX. So why are they part of the CubeMX repository environment.  For example, I am currently tr...
Posted on November 12, 2015 at 15:04In the current release of CubeMX V4.11.0 using the latest F4 libraries, V1.9.0, a bug has been introduced that makes the SDIO DMA channels useless.  In the previous library set, V1.8.0, when the DMA channels were ...
Kudos from