Hello all , we use stm32f072.1.is this regulator LDLN025M33R can be alternative for LD39050PU33R no legssince we would like to use his "legs" .our current conception is 90mA 3.3V .thanksyaniv
we using raspberry pi 4 to run Apache python , mysql an c kernal and it runs excellent om 4 Giga ram.we would like to move to stm32p1 , can it being compare and be replaceable ?
when pwr is down and only vbat is connected. the RTC freeze (TIME STOP) WHEN PWR IS ON IS Continue , please send please send HAL code example stm32f072 configuration thanks
Hello ,1 i would like to save user configuration into the flash of STM32F072 into pages . ( it few Kbytes )2. reading : RM0091 Reference manual I saw the pages space - but how do i know what flash pageas are available for save data.3. i use k...
Hello Clive ,thanks you for your time TO answer me , looking at the .map as you said i see few "blocks " of Rom 2.1 is Image Entry point : 0x080000c1 is FLASH Region _IROM1 () just to be 100% sure ? Image Entry point : 0x080000c1 Load Region LR_...
Posted on June 29, 2018 at 07:29thanks for your answare ,1. still not 100% cear 'in case you need any of features below' do you mean below 1.8V meaning power source is 1.7V ?2,we use use vdd as 3.3V so PDR_ON should be tied to vss (gnd) thanksyaniv