User Activity

Hey guys,I have connected two ST eval boards with my PC running Windows 10 v1803. When I connected NUCLEO_L432KC it was recognised as a COM port in the device manager and in "This PC" it showed up as a device and contained a txt file and a HTM file w...
Hey guys,I am using a STM32 F411E DISCO board and downloaded ST FP AUD_SMARTMIC1 library to learn audio feedback suppression caused by a mic and a PA ampliflier nearby. In the library C files given in the projects folder of FP AUD_SMARTMIC1, they are...
Hey guys,I used ST CubeMX(v5.2.0) with TrueSTUDIO IDE in Windows 10 PC. My work is to generate a new project for STM32 F411E DISCO board and tweak and implement the examples given for STM32 F446RE board in the ST's FP-AUD-SMARTMIC1 software's projec...
Hey guys,I have connected two ST eval boards with my PC running Windows 10. When I connected NUCLEO_L432KC it was recognised as a COM port in the device manager and in "This PC" it showed up as a device and contained a txt file and a HTM file with th...