Hi, I posted the original request WBW(way back when) and I found the solution I don’t use TouchGFX anymore Ps you can remove me from the distribution list of touchgfx
Hi Martin,
That didn’t go as well as you indicated!
Here is what happened:
· Changed field “APPLICATION DIRECTORY�? from “C:\TouchGFXProjects�? to “V:\TouchGFX�?
· Created simple project 2 screens one button each that switches...
Posted on November 23, 2017 at 14:07Your results may not be as bad as you think. With 0V applied the largest deviation is 45mV or 1.5% of full scale(3V). Your voltmeter will read between 2% to 5% of full scale depending on make and model. This is v...
Posted on July 28, 2017 at 03:24Hi,Here is what you need for this: you need to clock the timer to get a resolution of 1degree using the system clock and prescale registeryou use the zero crossing to trigger the timer start (this will happened 2 ti...
Posted on April 27, 2017 at 12:27I think there is precedence involved:your instruction could be TIMx->CR1 =(TIMx-> CR1 | 0x1) <<3;or it could be TIMx->CR1 =TIMx-> CR1 | (0x1 <<3);I believe you want the latter one and since...