User Activity

Posted on December 26, 2015 at 07:27Hi All,Been awhile since I used SPC5Studio, version 1 I think. Has eTPU2 support been added? If not, are there any plans to add it and on what time frame?I really liked SPC5Studio, however in my application eTPU2 ...
Posted on September 13, 2014 at 00:50Hello All,Our next project will be using the SPC564A 324 pin processor. 1. Can ST provide the schematic symbol and footprint in Altium library format?2. Can ST provide the schematic symbol and footprint in any li...
Posted on August 04, 2014 at 17:22Are there any example projects for the SPC564A on the SPC56xxMB EVAL board that show how to use external RAM?If not complete projects, any code snippets or even hints or advice?ThanksKevin
Posted on November 11, 2013 at 04:06Pad configuration information is needed for the SPC56xxMB EVAL board with the SPC 564AADPT324S mini-module. On the SPC564A (324 pin package), almost all of the eTPU2 and eMIOS pins are multiplexed. For example, on...
Posted on July 17, 2013 at 16:00In the course of learning SPC5 Studio I modified the Makefile and rules.mk to output a Motorola srec (.mot) in addition to the regular outputs. This can be very useful for those of us with a Motorola/Freescale backgro...