User Activity

Hey,im going to use the STM32h743 uCIn case the SW got stuck, is it possible to reset the program internally ?i would like "to save" implementation of External HW Watchdog. Moreover, do you have any recommendation for external HW circuit for Watchdo...
Hey,in my application, ill have an RTC function, that should work also when power in down.From this reason, I’ll use a battery that will be connected to VBAT pin.My question is about LSE clock.my plan was to connect an external oscillator 32.768kHz t...
Hello,as I see at the AN5200 only in DS and HS the signal level is 3.3V.Does it mean that the IO signal level in SDR50 for example will be 1.8V on the host side?The MCU has internal LDO for it ?Or the host size is always 3.3V, and the signal voltage ...
hey,as i saw at the EVB, the driver uses the SDRAM as a memory source for the RGB interface.the SDRAM size is 256Mbit while the SRAM is 16Mbit.in my application, my plan is to use the SRAM only.Do you see any problem to use the SRAM memory for the RG...
In my Application, ill use 2 uC stm32h743.Between both, my plan is to apply a SPI interface, when one of them will be the Master and the second will be the Slave.My first question is, does the uC can work as Slave? does clk pin can work as input at t...