User Activity

Hello I am using ST MCSDK 5.2 for a bicycle hub motor (with freewheeling) and try to tune the startup parameters.I get decent startup by activating "rev-up to FOC switch-over" The downside: If the motor is still moving from the last run and I try to...
Hello!I would like to use the ADC4 of a nucleo303RE board with a X-NUCLEO-IHM08M1.The Software (MCSDK 5.1.3) has functions already written for this in mc_tasks.c:void MC_RequestRegularConv(uint8_t bChannel, uint8_t bSamplTime)uint16_t MC_GetRegularCo...
Posted on May 23, 2018 at 16:57Hello,I am working on running a 250W Hub motor with the following setup:STM32F446 NucleoX-NUCLEO-IHM08M13 Hall sensorsunfortunately the Motor Profiler fails to profile the motor I am using and so I measured and entered...
Posted on May 14, 2018 at 16:13Hi,When not using the motor profiler and instead writing all details by hand into the Motor Control Workbench (with Hall Sensors, Manual editing of PI variables disabled) at Motor - Parameters, there are fields for Ine...
Kudos from