User Activity

Hello everyoneIn my Motor Control application I use low side active low gate driver L6398. Because of the shortage of this component, we need to use L6399 in which low side gate driver is active High.We developed application using Motor Control Suite...
Hello everybodyI'm using ST Motor Control 5.4.1 to drive a BLDC motor. It works fine, and I'm able to drive in SPEED MODE my motor, changing speed and with the system that can react to load changes.I would like to realize a software limit, so I can l...
Hello everyoneI'm trying to control a motor using STC_SPEED_MODE. There's a problem at startup: I program a ramp (for example i would like to obtain 6000RPM), motor start to rotate and accelerate, but speed reach maximum speed for the motor (for exam...
Hello EveryoneI'm using FOC control for a BLDC motor. It works fine, but there's a situation that I can't solve.I'm using a trigger as input: when pressed, the motor starts and must remain running until the trigger is released. If the user press the ...
Hello everyoneWe use ST1S14PHR to reduce from 40V input to 15V output. 15V are used to drive Mosfet (BLDC Motor Control). Lately we had a lot of problem with ST1S14PHR, because some parts failed during on field operation. We cannot understand what is...
Kudos from