Starting server with the following options: Persistent Mode : Disabled Logging Level : 1 Listen Port Number : 61234 Status Refresh Delay : 15s Verbose Mode : Disabled SWD Debug : Enabled InitWhile...
Should the be a 3,3 voltage in NRST pin. as far as I can tell the pin is low all the time. (Connected it led without resistor and still nothing).Do you think the board maybe faulty?
The STM32CubeProgrammer connected when I set the ST-Link mode: Hot plug. Still the Full chip erase fails.Other modes have the same problem as earlier descriped.