User Activity

Posted on March 18, 2018 at 18:06 Hello, I want to use the ADC and the DMA on Simulink as follows: The ADC is triggered by the rising edge of Timer 2 which generates a PWM signal with a frequency of 100 kHz. So, I want to retrieve the 132...
Posted on March 12, 2018 at 17:10Hi -- I use 2016b Matlab version with STM32F429ZI nucleo board. I am tring to use External mode with simulink, I followed the example and the instructions decribed in ''the MAT/TARGET instruction (Hands On, Rev 2.2,...