User Activity

Hello everybody,I use the STM32H743 and try to flash it via UART, which usually works quite well.I would like to know whether it is important to de-energize the controller before connecting the programming adapter or the adapter must be connected und...
If I connect a constant rising signal at the ADC input, I observe significant fluctuations at certain ADC values. These fluctuations always appear at the same ADC values. The affected values have the following format XX500, e.g. 18500, 19500, 20500 e...