Hey @Trac3r,what versions of cubeMX & MCSDK are you using?MCSDK V6.2.1 & cubeMX V6.11 work pretty well if used together.there might be some issues when using MCSDK 5.4.8.regards
Hello @GMich.4 I think the PHASE.x pins are fed to the MCU because we have a resistive divider before it, so they must be the three phase voltages of the motor being scaled-down.If you want to observe the real phase voltages of the motor you should c...
Hello @mikde The procedure I follow to profile a motor:1.Choosing a random motor, the power board, and the control board.2.Checking motor profiler in the workbench3.Reducing the baudrate of the USART to 1152004.Reducing the PWM frequency from 30kHz t...
Hey @ACho.11 if I understood correctly, you could choose the STEVAL-ESC001V1 as your inverter board in the MCSDK V6.2.1 and use the ST board manager, make a clone of it, then modify it based on your own hardware. They must be quite similar.More infor...