User Activity

I see that ST2100 is active but it seems there is no stock in anywhere.I only see datasheet but, are there more documentation, application note, evaluation board for this broadband PLC Soc?Thanks in advance!.Best regards.Francisco Jimenez.
Hello. I try tu adjust the value of shunt resistor in STPM10 electronic circuit.First I placed one 0.5mOhm resistor value, and I watched that 40W lamps meassurement is not very exact. Maybe I should to increase this value. But I have read that maxim...
I have noted in my program following behaviour.Fist time microcontroller is programmed with entire FLASH erased before, Program runs right.If I disconnect device or it is reprogrammed, PWM does not work.PWM will work again if previously, all FLASH is...
I want to develop 6LOWPAN over S2-LPThis mesh network have other devices that support 6LOWPAN, different to ST microelectronic manufacturer. Could I tune S2-LP in frequency, band, modulation, etc in order to can speak/listen with other devices?Best r...
Posted on May 11, 2018 at 13:28Hi all, I'm using a STM32F215 MCU with a supercapacitor (like XH414HG-IV01E;SEIKO) connected to Vbat through a 0 Ohm resistor in order to backup RTC registers. I attach an image:Well. If I measure the voltage in VBAT p...