User Activity

I'm pleased to share stm32mp-sign-tool with the community : It is a lightweight open-source alternative to STM32_SigningTool_CLI that does not require the full STM32CubeProgrammer installation and dependencies. GitHub Repository: https://github.com/e...
Hi, when trying the new ST BSP release base on linux kernel 6.1.82 on my stm32mp157f-dk2 I noticed that the legacy framebuffer support is not working anymore.this was working perfectly on the previous release with linux kernel 6.1.28.I didn't succeed...
Hello, I use Optee on a stm32mp157f-dk2 board, version is the and the corresponding BSP :optee-os 3.16.0-stm32mpu-boot v2021.10-stm32mpLinux v5.15-stm32mpAll my changes are committed and built using a yocto meta-layer : https://github.com/embetrix/m...
I have a custom board based on stm32mp157c which is working with arm-trusted-firmware version v2.2-stm32mp.I updated tf-a to version v2.4-stm32mp version keeping the same DTS file but the problem is that tf-a is starting and hangs at loading sp min a...
hello I have build tf-a and u-boot and signed them as specified in the st wiki documentation:But I get the following error when booting up:NOTICE: CPU: STM32MP157FAC Rev.Z NOTICE: Model: STMicroelectronics STM32MP157F-DK2 Discovery Board NOTICE: B...
Kudos from
Kudos given to