Hello Mr. Mora, I think the best easier way to make some demonstration is with FP-IND-PREDMNT1 - STM32Cube function pack for multi sensors node with signal processing to enable predictive maintenance - STMicroelectronicsFP-AI-PREDMNT2 - STM32Cube fun...
Hello,I think it is clear from the code you shared that from the .ucf file it is also possible to convert this sequence of values to a header file (.h) to be imported in any C project (e.g. driver, firmware, etc.): Unico allows .h file generation (fr...
For SPL (Sound Pressure Level) measurements we would recommend digital microphone such as IMP34DT05, it is more simpler to implement with this vs analog microphone.SPL level measurement reference code is available in FP-AUD-SMARTMIC1, this could be r...
This is not very easy to say, it depends on the mechanical construction monitored and its evolution in time towards the maintenance need. ST does not have any specific SW for this.
The measurement bandwidth of the digital MEMS microphones in ST portfolio is covering audible bands or let's say frequencies up to 24kHz approximately. For the Analog MIC the band is not limited by the digital conversion and therefore sensing up to 8...