User Activity

Hello,MCU - STM32F746NGH.FreeRTOS.I'm trying to interface with 2 external single ended ADC (texas instruments ads8660 - http://www.ti.com/lit/ds/symlink/ads8860.pdf). The ADCs are connected via SPI2 and SPI3 respectively. The ADC can sample at a ...
Posted on May 02, 2018 at 18:00Hi,I'm looking at trying to implement a USB host (MSC) driver using the high speed core on the STM32F746NG MCU, we do not have an external PHY so are using the embedded PHY.  How does one achieve the 5v required for VB...
Posted on April 06, 2018 at 15:05Hello,STeMwin version 540.FreeRTOS version 9.0.1.IAR EWARM 8.20.1STM32F746NG with 32MB of external RAM.I'm trying to use STemWin in a multi-task environment however I'm not getting very far.  I had actually been usin...
Posted on February 07, 2018 at 17:41Hi,We are running a system with a single F7 I2C master and a number of F0 based I2C slaves (currently 4 slaves), each slave is connected to the master via ~0.3m cables.  We are using 10-bit addressing.We are seein...
Posted on January 12, 2018 at 13:55Hi,We are using a 216Mhz F7 (STM32F746NGH6) on a custom board to interface with an LCD (Winstar WF70GTIAGDNG0).  We are having issues with the screen flickering, often the screen will display a flickering green blo...