by referring "http://www.techplayon.com/lora-device-activation-call-flow-join-procedure-using-otaa-and-abp/#:~:text=By%20Personalization%20(ABP)-,Over%2DThe%2DAir%20Activation,below%20depicts%20the%20join%20procedure.", I found my mistake which I did...
@Community member Thank you very much for the detailed quide. According to the module(shield) manual, we need to reset the module after chaning the band. But, actually, we don't need the reset. When I first tried your suggestion, even though the ba...
the manual is unclear in that point. It's usual that you can't see any thing in teraterm since the UCLEO board and the "I_NUCLEO_LRWAN1" are communicating each other via UART interface as default. If you put the AT Master project as it is on the sen...
I am on your side that the guide or manual from ST is just for using the kit as it is. They lacks on the key information to change any parameters of the LoRa module (especially the sensor node side). Even though we can use AT commands for the LoRa Mo...
I have similar problem, and I don't have any idea on the procedure to change the band. Is it enough to call the function alone or we need to reset the module? It would better if the manual describes the procedure more in detail.