User Activity

Hello,I am trying to compile the Openst Linux for my custom board. I did it succeed in the Kirskstone distro which is based on tf-a. Now I try compiling the latest Openstlinux (6.0, scarthgap) with the optee-os but encounter a problem with the file g...
Hi,I have a small problem with the RTC on STM32MP153. From hardware point of view I'm able to see sine waveform on the resonator 32.768kHz which is connected to PC14, PC15.I use the Openstlinux - kirkstone (openstlinux-5.15-yocto-kirkstone-mp1-v22.11...
Hello,currently, I'm in the production phase of my product which is based on stm32mp153. Unfortunately, I have a huge problem with setting the password for root.First I commented debug-tweks in local.conf.I added  INHERIT += "extrausers" EXTRA_USERS_...
Hi,I use in my project STM32MP153, which is a model without a GPU. My application also doesn't need any graphical representation like Wayland, X11, etc. How can I update st-image-weston.bbappend to remove these unnecessary elements?ThanksMW
Hi,I have a problem with hanging up my board occasionally when an issue from the console reboot.I read about and the internet says this is a problem with the EMMC memory's power cycle.So I followed by a linkhttps://github.com/orangepi-xunlong/openwrt...
Kudos from