Posted on September 14, 2017 at 16:28I agree, I'm not sure it's a HAL issue. What I'm saying is that with the new HAL, the SDIO/FatFS seem to be less stable than before. In my case, with the following 2 changes the writing to the SD card works fine:...
Posted on September 13, 2017 at 10:40I'm actually experiencing the same problem with some SD cards (ex. a 2GB Sandisk). I have an application that is compiled for both F4 and F2 uC that needs to read some files and write a log file to the SD card. I...
Posted on April 28, 2017 at 15:14 Hi st.mcu I tried v1.16 and it seem to work fine. Since the SD API changed and I'm sharing this code with a F2-based project as well, do you when when a new HAL for the F2 will be available? Many thanks!