Dear NajeemSyed X-NUCLEO-DRP1M1 are in Nucleo-64 form factor so it is dedicated to be plugged directly on a NUCLEO-G0xx or G4xx.this is ony in this case that you can use the X-NUCLEO-DRP1M1 BSP. Then in your case, you have to define required resource...
Hi Robert Thanks for your feedback and you are welcome, For ADC Isense, just enable a GPDMA for ADC4.Then usbpd_ADC.h should be like this:Also I saw in your .ioc that no RTOS is enable for the moment, please dont forget to enable TheadX. Best regards...
Hi Robert7Thanks for sharing your .ioc and project. As you are not using a BSP (which is correct), you should fill the platform settings tab of the X-CUBE-TCPP. This is why usbpd_ADC_SNK.h is missing. But the main point is that the B-U585I-IOT02A has...