Hi @PSuvi.1 I don't believe I run into this issue when installing WiSE-Studio on mine. The steps below are what I did to get it to work (there may be a few restarts in between those steps to get it to work).Install Java JRE/JDK 18 and make sure it i...
All good. Thanks for the help, @RArch .@Sebastien DENOUAL Do you think anyone can take a look at this issue? Not sure if this information is useful, but STM32CubeIDE runs on my mac perfectly fine (with no java installed).
@RArch I downloaded and installed the java v18, but it was a no-go still. I even tried to run it from command line, but it kept showing CheckForInstalledJavaRuntimes error (see attached). I will attempt it on an intel mac to see if it makes any diff...
I was able to use xattr to by pass "WiST-Studio.app" is damage, but still wasn't able to launch the IDE. I installed OpenJDK (version 17) but no luck. Then I installed jre-8u333 from java.com directly but still no luck. @RArch How did you install/up...
Hi Sebastien,Just confirmed on an Intel machine and it had the same issue. Below are the steps I used to try to open the file.Extracted en.STSW-WISE-MAC_v1.1.0.zip to wise-studio-1.1.0.dmg successfully. Double clicked on wise-studio-1.1.0.dmg which t...