User Activity

we have performed below following pre compliance test and found : -1) Radiated Emission : - Passed.2)     Transmitter Spurious Test : - Passed3)     Receiver Spurious Test : - Failed (Getting harmonics at 4.8 GHz of -38dbm in Receive mode at channel ...
As SPBTLE-RF module is already CE certified and I have its test reports also. But as a complete product we have to perform this tests again: -1) As per EMC EN 301 489-1 V1.9.2 / EN 301 489-17 standard: - a) Radiated Emission b) Electrostatic Di...
After once BLE Initialize and authentication set by fixed pairing key as "123456" then can we change again pairing key to "123678" by using this API "Aci_Gap_Set_Auth_Requirement()".Means BLE will disconnected and I will configure its authentication ...
After once BLE Initialize and authentication set by fixed pairing key as "123456" then can we change again pairing key to "123678".Means BLE will disconnected and I will configure its authentication fixed pairing key with other value during run time ...
Is it SPBTLE-RF (BLE) module can directly communicate with laptop Bluetooth although I have customized serial port profile. I tired after paring with laptop Bluetooth in device manager it not show any com ports/virtual com port. Can any one suggest h...
Kudos from