Hi @PhilippH , Thank you for your detailed comment. I'm fully agree with your assumptions.1-I confirm from our side that the Rx_Buff size should be at least equal to the number of descriptors and the maximum of Rx_Buff size could exceed the number of...
Hi @Community member , For LwIP_StreamingServer application : FPS is around 19.5 frames/sec Latency is around 1.5 secondPlease note that the application available under STM32Cube_FW_F7_V1.17.0 package need a fix (An Internal ticket ID 142051 is alre...
Hi @Community member ,Thank you for your request, Performance tests are in progress, We will keep you updated as soon as we have your required information.
Hi @PG.9 ,In order to understand well your issue, could you please clarify some points :when you say "you are able to assign Static IP", you mean that your IP instance address is affected than go to 0 ? Your IP instance address is affected only when...