User Activity

Hi.Chip: ST BlueNRG-345ACPCB: Custom board with VLXSD pin left floating and VFBSD pin ->3.3V, NX2520SA 32MHz, schematic mimics STEVAL-IDB011V1, just bare chip without MEMS or CMSIS_DAP debugger, just MCU, decoupling capacitors, chip-antenna with matc...
Posted on August 31, 2015 at 20:09Hi. Is it possible and if yes, where can i find examples how to communicate with slave devices that work only with  Repeated Start instead of Stop when reading them? Library: Cube F4 V1.3.2 MCU: STM32F429ZI
Posted on August 08, 2013 at 19:27  The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on August 02, 2013 at 22:54Hi to Alli'm trying to get to work the ethernet periphery in MCU, i can successfully init DP83848i , can read regiter, and even(i think) receive packets, but mcu does not transmit any packets outside. the code i've ...
Posted on May 08, 2013 at 22:51hi to all. can't get lib to work, tryed GPIO example but it did not worked on real mcu, tryed  in simulation mode where i see default value of registers, i've tryed example as is, without any changes.can't say version ...