Posted on May 17, 2011 at 09:56Hi, Just an idea : To write in the flash (Bank 0 as 1), the piece of code which do it HAVE TO be executed from RAM, never from Flash (including the other flash bank) Hoping will help you. Regards. damien HOYEN
Posted on May 17, 2011 at 09:56@lakata : Hum, you should look at the end of your development to implement the watchdog functionnality... My point of view is: before is always a lack of time, and complexify deeply the debuging... @sr_shinde: How do y...
Posted on May 17, 2011 at 09:56Hi, I was using both of VIC0 as VIC1, with FreeRTOS, with plenty of interrupt source (7 or 8). Both was working. Are you able to fire (more than 1 time, to be sure the return works correctly) a unique interrupt source,...
Posted on May 17, 2011 at 09:56hi, I m not an expert about embedded linux, but seems need a external memory controler, with ''huge'' quantity (in comparaison to the STR9 embedded 96K of RAM). Same idea with flash. Take a look with Atmel, they make s...
Posted on May 17, 2011 at 09:56Hi, If my memory is good (TBC), i had this trouble this is a BUG in the ST library: The previous interrupt is disabled before you install a second (), look the code in the timer, this bug is in the 91x_tim.c. Add a bre...