User Activity

Posted on February 10, 2014 at 10:39HiI'm using STM32F373x SPI in slave mode. I get errors in about 0.1% bits transmitted, occurs in 50% of units from first production series of custom board. SPI lines have RC filter installed to improve EMC immunit...
Posted on August 13, 2013 at 14:23Hi, I have a simple question regarding internal SRAM size of STM32F373Rx processor. Datasheet (rev.3, table 2 on page 10) specifies SRAM size of 24kB for 128kB Flash units,but I can read and write up to 32kB of SRAM...
Posted on May 17, 2013 at 10:09HiWe are using STM32F373 for the first time in our units and a problem with SDADC full scale occurred. We use it in a simple resistor measurement circuit:Circuit compares Rx with a know Rref resistor. Controller is sup...