Posted on May 17, 2011 at 13:00Hi All, Finally the new version of EWARM (v5.30) is released! You can downlaod it from : http://www.iar.com/website1/1.0.1.0/68/1/index.php? It supports many new features, for more information refer to: http://www.iar....
Posted on May 17, 2011 at 12:50Hi, The watchdog and timer suppott means that during a breakpoint, you have the possiblity to choose how the counter of timers and watchdog should behave: â—� they can continue to count inside a breakpoint. This is usu...
Posted on May 17, 2011 at 12:49Hi everybody, Good news! Hitex will release a new version (in the few coming days) of HiTOP-CTX (build 5.30.0014). In addition to the serial viewer which is already supported in the last release, Hitop 5.30.0014 will p...
Posted on May 17, 2011 at 12:49Hi all, you can store code in Ram using pragma with tasking compiler. What you should do is enable ''long branch veneers'' from the linker options, because without this option the pragma doesn't work. good luck:)
Posted on May 17, 2011 at 12:42Hi, Let's begin with HiTOP and TASKING compiler. Technical support: excellent. Feature : very good: In addition to the basic debugging features, HiTOP supports many other features such as serial wire viewer(semi hostin...