Posted on May 17, 2011 at 13:12Hi, I'm sorry but I lost track with the forum the past couple months. But to answer your question, yes we resolved the issue. It had nothing to do with the code. It was purely a hardware issue. If you are still struggl...
Posted on May 17, 2011 at 13:12Hi there! So we captured a basic transaction on spi3 and then compared it to the one on SPI1 After the level translator we still see the same signal, nicely shaped but just on a lower level. When we measure the MISO on...
Posted on May 17, 2011 at 13:12Hi, We bring SPI3 out to ext header pins and connected a radio directly to this one. Brought down the voltage to 2.5V so we could leave the level translator out. Didn't change anything in the code just changed the inte...
Posted on May 17, 2011 at 13:12Hi, I only have send you a part of the design but we have some other stuff also running on the board that require a 3.3V and since we had more devices that require 3.3V it was better to run on 3.3V because then we don'...
Posted on May 17, 2011 at 13:12Uhm my VccA is 2.5V and my VccB is 3.3V So i'm pretty sure that VCCA is <= VCCB :-D. You got me really confused for a second! Greetz, Wova [ This message was edited by: wouter.vanaken on 18-05-2009 23:31 ]