Hello,Overall documentations regarding the use of PLS UDEDEBUG normally is under its installation pathC:\Program Files (x86)\pls\UDE Starterkit 5.0\ManualsThis above path depends of your UDESTK tool version installed.Regarding the SPC5Studio document...
Hello,you can follow two roads to acquire these concepts:look at the documentation present into SPC5Studio itself clicking on: Help -> Help Contentslook at youtube SPC5Studio available demos and applications.Hoping this help you.Regards
Hello,As reported by the RM ...When the watchdog is disabled (SWT_CR[WEN]=0), this field shows the value of the internal down counter. When the watchdog is enabled (SWT_CR[WEN]=1), this field is cleared (the value is 0x0000_0000). Values in this fiel...
Hello,I have already fixed the issue and internally delivered the solution. You will find it on next set of SPC5Studio updates planned for the end of January.Regards