Posted on May 17, 2011 at 13:15Here what I have done and am trying to do: 1) I have a IAR STM3210B - SK EVM loaded with the example workspace called IAR-STM32-SK and project titled virtualcom loaded to flash on the EVM. The LCD message says it is th...
Posted on May 17, 2011 at 13:15How do I get tech help on the STM32. The on line entry system seems to have an error every time I put in a request. When I contact Arrow they say contact ST and ST does not have a system to help with thier products. Jo...
Posted on May 17, 2011 at 13:15I have it working. The clue was the CD class device name. The Virtual Port Comm wants it to be a different designation. I used a code example from ST for the STM32, modified it to work with the IAR EVM and it configure...
Posted on May 17, 2011 at 13:151) I have a IAR STM3210B - SK EVM loaded with the example workspace called IAR-STM32-SK and project titled virtualcom loaded to flash on the EVM. The LCD message says it is this project. 2) Using the VCPDriver_V1.1_Set...