Posted on May 17, 2011 at 12:22Hello, I'm using Crossworks with segger j-link. I have a problem to erase flash where the downloader writes the application code. I try to erase it also manually (with 'erase all' command) but it is not erased. Is ther...
Posted on May 17, 2011 at 12:22Hello, I have already downloaded and installed the component package 1.2. When I try to download the .elf file into the flash memory with segger j-link, it saves correct bytes from 0x08000000 to 0x008005d3 and no corre...
Posted on May 17, 2011 at 12:22Hi, Thanks, but the problem continuos to be present. I have downloaded the component package v.1.2; the .text segment starts from 0x08000000 but the download phase ends with message 'verify error'. The .elf file is dif...
Posted on May 17, 2011 at 12:22Hello, I'm using Crossworks for ST CORTEX-M3 with Segger J-LINK. When I download a .elf file into the STM3210B-EVAL evaluation board, it begin to download and at the end it shows the message 'verify failed'; the code s...