Posted on May 17, 2011 at 10:15hi there, i have a problem with the over current mechanism of the ST7FMC2. The problem is, that its not possible to start the motor after an CL_Interrupt in the opposite direction. A restart in the same direction works...
Posted on May 17, 2011 at 10:14Hi Gigi, thanks for your help. We solved the problem with a fix duty cycle and small modifications in the mechanics. For me is the problem in the Z interrupt a bug of the controller. The sensors are not oscillating. Ma...
Posted on May 17, 2011 at 10:14Hello, so far so good. Now I`m able to hold the position with a fix duty cycle in direct access. When I use a duty more then 30 %, the motor is going very hot. I use a 24V motor and at 30 % there are about 700 mA curre...
Posted on May 17, 2011 at 10:14Hi, you are right, when I prevent the start, if the motor is not still, the endless loop will not occure. But I have to prevent, that a User is possible to change the position of the motor. So, this solution will not w...
Posted on May 17, 2011 at 10:14Hi Gigi, 1.) I have this problem in a lot of different cases. For example, when the motor have to start with a heavy weight and the torque is not enough. As well in the case, the motor is stopped, in motion and I like ...