Posted on May 17, 2011 at 09:40Hello, I've tried your tips, but it doesn't work. I have got TIM0-Int for 1ms regularly. It works for so long, I don't get an RX-Int. After this IRQ-Handler, the Timer has the OCFA/OCAIE- bits are set, but the Int is n...
Posted on March 27, 2009 at 10:17Hello, the problem is solved. In the flash.h the FLASH_LOCK, FLASH_BSYAx are numeric, not bits. Therefore I've tested the wrong bits in CR0.:-[ Greetings, Steffen
Posted on March 26, 2009 at 05:02Hello, I try to initialize my Flash. I've learned to do this from RAM. But after this, it should be possible to set INTM in FLASH->CR0?! The following code prints: count = 4 thus I have to write 4x the Register CR0....
Posted on March 18, 2009 at 06:50Hello, I'm fighting with spurios resets yet. After Reset, the WKP_RES is always set. The WAKEUP-Pin is used for XTI ISR (P0.15) in my Appl. According to the Ref. the Pin is ''functional'' after PowerOn-RESET. The P0....
Posted on March 12, 2009 at 05:04Hello, I've just found this tree. I'm using the IAR 4.42A toolchain. Is the problem active yet? BTW: Raises the Erase-Op an Inter- rupt too? regards, Steffen