Posted on May 17, 2011 at 09:36Evidence of people building str9 images using gnuarm is conspicuously absent from the internet. People are using IAR, and KEIL. Even FreeRTOS only uses IAR for str9. How can it be a Free RTOS if it needs a commercial c...
Posted on May 17, 2011 at 09:36Date code 620. It seems unlikely to be a defective device. The problem seems to lie with the compiler. Replacing the part would be difficult and have no more chance of success than installing the original part. The mos...
Posted on May 17, 2011 at 09:36Now they're all connected and it still doesn't work. Suspected the extra pins were for routing convenience because they're all shorted.
Posted on May 17, 2011 at 09:36Do all the Vdd, Vss, Vccq, Vssq pins and Vbat have to be connected to get the STR91x running? Currently only one Vdd, Vss, Vccq, and Vssq pin is connected and it isn't running anything. Only JTAG works.