Posted on May 17, 2011 at 13:21No help Your Flash Programming manual says: '' The in-circuit programming (ICP) method is used to update the entire contents of the Flash memory, using the JTAG, SWD protocol or the bootloader to load the user applicat...
Posted on May 17, 2011 at 13:21I have STM32F103VC and VD devices. I need to develop a model for an in-circuit tester that will program the flash through the JTAG port. I have the Flash Programming Manual PM0042, that shows me all of the FPEC registe...
Posted on November 13, 2006 at 18:08Najoua, Your last advice seemed to work, I was flipping the wrong bit in the SYSCON. I still had one instruction that hangs the ST10 (see below). However when I commented this one out I was able to access all of t...
Posted on November 08, 2006 at 11:30Adding to the last message. I think I have a theory as to why this might happen to me. See last message. I send a 00 to the ST10 through the UART to start the BSL and set the baud rate. The ST10 replies with a D5 ...