Posted on May 17, 2011 at 12:27Hi Mike, it seems that with some google-ing, you can find the new part no. The new devices will only be available in packages of 64,100 and 144 pins. Have a peek at http://www.best-arrow.com/2_STM32CortexUpdate MAR08.p...
Posted on May 17, 2011 at 12:27Hi Mike, I am a distribution FAE, so we get this info a bit before it becomes commercially available. These devices are in beta test at some keycustomers, so its not just paperware. I have the new part no, but not sure...
Posted on May 17, 2011 at 12:27Correct, I2S is foreseen in the new devices, but only on the performance line. To be more detailed: Access line will have 5*USART, 4*16bit timer, 3*SPI, 2*I2C, 1*ADC, 2*DAC and EMI. Memory up to 512K Flash and 48K RAM ...
Posted on May 17, 2011 at 12:27Forgot to mention that the for 1Gb, NAND flash might be the cheapest solution. These days, you have managed NAND ICs with embedded NAND controller with MMC interface. As you might know, the MMC interface also works wit...