Posted on November 17, 2006 at 04:34I found out that the information is located on the package/box. It seems that we have some in the production that are only 245ºC, and the latest received from the supplier are 260ºC.
Posted on November 16, 2006 at 15:37Hi I cant find any information regarding the reflow peak temperature for the LQFP 144 package. Please advice? Best regards Thomas
Posted on June 09, 2006 at 09:20great CAN_TIMING( 5, 4, 3, 2) seems to work! My problem was that I made a mistake when calculating the total number of TQ. Thank you very much for your help!
Posted on June 07, 2006 at 12:50I have to re-calculate the CAN bit timing which is implemented in the CAN library, as I switch the APB frequency between 48MHz and 2MHz (PLL off). I've changed the baudrate prescaler as the library assumed 8MHz APB. I...