Posted on September 14, 2005 at 06:53Hi Jimmey, I have implemented the basic circuit on a board (except the reset circuitry which is a bit different) and it works fine. I had to reduce the JTAG speed a little but maybe it's due to the length of cabl...
Posted on August 05, 2005 at 09:10The values are not explicitely written in the Reference Manual, but you can calculate them using the information in the Device Pin Description table (see page 22).
Posted on July 26, 2005 at 11:02Sorry to bother you again Hich, So if I understand correctly your reply, - All I/O pins switch to high-impedance - All registers values are preserved - Only the RAM is cleared Right ? 8-)