Posted on May 17, 2011 at 12:08hi all, I want to port the real time operating system uc/OS-II to the uPSD3234, but have no idea whether it supports porting? Anyone have done the similar job? ...hope someone can do me a favor, thanks.
Posted on May 17, 2011 at 12:07Thanks for your reply. In my application I want to save a counter in the Flash Memory so that I can retrieve the counter after power-down and on. The counter may be read and write in an fixed address very offen, so I w...
Posted on May 17, 2011 at 12:07Hi all, I'm using uPSD3234 to develope an application. I want to know the life time of uPSD3234's Flash Memory. How many times can I write or erase the Flash Memory till it fails to read and write correctly? Thanks.
Posted on May 17, 2011 at 12:06I know there are several formats of file concerning the uPSD3200 programming. The first one is hex-80, which is user's firmware and generated by a compiler such as KEIL; The seconde one is obj, which is the output file...