Posted on May 17, 2011 at 10:18check your power supply it seem that u don't have egnouh power are using Batterys ?? the Vs = 20V MOTOR VOLTAGE the VSS = 5V TTL/CMOS[ This message was edited by: Cortex on 05-04-2005 00:30 ]
Posted on April 07, 2005 at 21:21no need and why u use a OSC in MCU Then ?? u must send data and do some Delay() using Internal Osc (count the Cycles) and the Receiver will Read and wait the same Delay
Posted on April 05, 2005 at 16:07u can use the interruptions. fix a Normal State : ex : low and when u want to communicated change Input to Output and send the the data the other side will be in input and will go to interruption code i hope that you...
Posted on April 04, 2005 at 20:561 is the mininum ; One Wire 2 : I2C/SMBUS 3 : 3-Wires/SPI if you use many pins you get more speed but why using many Pin when the Microchip's Pic can be used to do something else while the ST7 do something more impor...