Posted on May 17, 2011 at 12:15Thank you. I could find no mention of this in the datasheet. Perhaps on the next revision it could be made a little clearer or more prominent that both can't be used at the same time. many thanks Ben
Posted on May 17, 2011 at 12:15In the USB and CAN thread you stated that ''in the STM32 the USB and the CAN shares the same RAM memory for data reception and transmission. So it’s not possible to run both of these two communications peripherals at...
Posted on May 17, 2011 at 12:15I would have to agree that according to the datasheet, they use different memory areas. Of course the datasheet may be wrong
Posted on May 17, 2011 at 12:15it looks as if you can only use both in hte 64+ pin versions. see page 87 of the programming datasheet. IT explains about remapping CAN I/O