Posted on December 09, 2004 at 09:43Another question regarding the ADC. The AD inputs will measure signals between 0v - 2.5v. But what about signal levels 2.5v - 3.3v? Will they result in the same value as 2.5v? (4096) or will the result be unpredic...
Posted on December 09, 2004 at 06:14Hi, In table 30 (page 142 in the reference manual Rev4/Oct2004) it indicates that pins P2.8-P2.11 acn be used for external interrupts. But when looking at table 1 (page 24) only P2.8-P2.10 has the alternate functi...
Posted on December 08, 2004 at 05:59Hi Hich, Ok, I see that it says that the /SS pin must be asserted high. But why???You say: ''to make sure there isn't more than one master at the same time'' But I still dont understand, I slave mode the /SS pin i...
Posted on December 07, 2004 at 08:14We are designing our hardware right now and have one question regarding the BSPI pin /SS. We will use one of the BSPI ports to clock data into and out of a large shift register. For that we will use the SCLK, MISO...