Posted on May 17, 2011 at 11:37General question: a cycle ''for'' how much delay inserts? or better how many cycles of clock employ? Example: for(i=0;iI use St92f120 with INTCLK 20MHz and compiler GCC9 of tool the ST9+VisualDebug. I do not succeed in...
Posted on May 17, 2011 at 11:37Thanks Sergio!!! You have reason because it is the only one pin that it had the various voltage in the two circuits. Now they work. But the pins that I do not use, as an example AD\ DS\ RW where I must connect them? I ...
Posted on May 17, 2011 at 11:37I have a problem with two identical circuits that use micro st92f120. The systems work with an external quartz to 4 MHz and INTCLK 20MHz. The first one works correctly. The other system goes reset every three second on...